Am trying to run standalone program(hello_world.bin) in u-boot.
U-Boot 2015.04+fslc+g5d9ffd2 (Apr 14 2016 - 13:05:07)
CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
Reset cause: POR
I2C: ready
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
auto-detected panel HDMI
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 1 not found
PHY reset timed out
FEC [PRIME]
Hit any key to stop autoboot: 0
=> fatload mmc 0:1 0x40000 hello_world.bin
reading hello_world.bin
606 bytes read in 13 ms (44.9 KiB/s)
=> go 0x40000
## Starting application at 0x00040000 ...
prefetch abort
pc : [<00040004>] lr : [<8ff6071c>]
reloc pc : [<878e5004>] lr : [<1780571c>]
sp : 8f54ad68 ip : 00000030 fp : 8f54c788
r10: 00000002 r9 : 8f54aec8 r8 : 8ffa6fdc
r7 : 8f55e770 r6 : 00040000 r5 : 00000002 r4 : 8f55e774
r3 : 00040000 r2 : 8f55e774 r1 : 8f55e774 r0 : 00000001
Flags: nZCv IRQs off FIQs off Mode SVC_32
Resetting CPU ...
resetting ...
After this it will reload the u-boot again.
I have tried with different addresses but in some it will get reset. And some others it will get stuck at
## Starting application at
Please get back as soon as possible.
解決済! 解決策の投稿を見る。
Take the following as the reference:
http://www.denx.de/wiki/view/DULG/UBootStandalone
https://github.com/lentinj/u-boot/blob/master/doc/README.standalone
According to the second link, seems that you have to load and run the application to the 0x0c100000 address for the ARM architecture.
Hope it will be helpful.
Basically, don't forget that Uboot is just a bootloader, not an OS, and it is not meant to run a complicated applications.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Not worked for me. I'm using Toradex Apalis imx6 board
Take the following as the reference:
http://www.denx.de/wiki/view/DULG/UBootStandalone
https://github.com/lentinj/u-boot/blob/master/doc/README.standalone
According to the second link, seems that you have to load and run the application to the 0x0c100000 address for the ARM architecture.
Hope it will be helpful.
Basically, don't forget that Uboot is just a bootloader, not an OS, and it is not meant to run a complicated applications.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------