Failed to execute MI Command:

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to execute MI Command:

6,801 次查看
sortiz
Contributor I

I build and debug NXP examples fine on IMXRT 1050 dev board, if I disconnect the board every single time before debugging. Next I terminate debug mode, i change the code,build, and debug without disconnecting the board and get this error. 

pastedImage_1.png

Thank you for your time, 

Steven O. 

2 回复数

4,917 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Steven

such error usually happens when previous debug session was not terminated propely,

one can check suggestions for this on:

GDB Debugging with Kinetis Design Studio 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,917 次查看
sortiz
Contributor I

This document was very useful for debugging, yet I had the same error. 
This update is for future people that may have the same problem. I had version v10.2.0_759.

I resolved the issue with installing a new MCUXpresso Verision- v10.2.1_795. 

Thank you, 

SO

0 项奖励
回复