FUSE_PORx bits of MMPF0100.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FUSE_PORx bits of MMPF0100.

ソリューションへジャンプ
804件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about MMPF0100.

MMPF0100 has FUSE_PORx bits , however there is no description about these bits in MMPF0100 datasheet (Rev.7.0).

Could you let me know the function of these bits?

Best Regards,

Satoshi Shimoda

タグ(2)
0 件の賞賛
1 解決策
664件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct, any of the FUSE_PORx may be used, no difference between them.

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
664件の閲覧回数
Yuri
NXP Employee
NXP Employee

OTP fuse bit FUSE_POR can be blown so that upon subsequent power cycles, the start-up sequence

is chosen from the OTP fuses and not from the TBBOTP registers.

664件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Yuri,

Thank you for your reply.

Then, I want t to know the difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3 also.

I guess the start-up sequence is defined as below.

If this is correct, there is no difference between FUSE_POR1, FUSE_POR2, and FUSE_POR3.

Is this right?

FUSE_POR.png

Best Regards,

Satoshi Shimoda

0 件の賞賛
665件の閲覧回数
Yuri
NXP Employee
NXP Employee

Correct, any of the FUSE_PORx may be used, no difference between them.

0 件の賞賛