Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)

ソリューションへジャンプ
1,738件の閲覧回数
Samhitha_Kashyap
Contributor III

Does NXP provide the Ethernet Driver for NXP i.MX8MP supporting FreeRTOS (CortexM-7)?

The variscite board var-som-mx8mp board has both the ethernets made available for the Cortex A-53 ( OS: Linux), I need to use one of the ethernet for Cortex M-7 ( OS: FreeRTOS).

Can anyone help me find the driver for the same.

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,718件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,719件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

The Cortex-M Core are mainly intended for real-time application, delegating the high-speed communications (like ethernet and USB) to the Cortex-A cores.

With the above into account we do not provide an ethernet driver for the Cortex M7.

Best regards,
Aldo.

0 件の賞賛
返信