Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable kernel configuration options like CONFIG_PROFILING and CONFIG_PERF_EVENTS

1,507件の閲覧回数
mohamad-ahmad
Contributor III

Hello,

Can someone help me how I can change the kernel configurations by enabling certain of them like CONFIG_PERF_EVENTS and CONFIG_PROFILING.

Normally when I check some configurations I find, for example:

# XXXXXX is not set

or

YYYYYY=y

Thank you for the help

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

935件の閲覧回数
mohamad-ahmad
Contributor III

thank you Yuri.

Mohamad

0 件の賞賛
返信

934件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The following may be useful :

Task #5 - Kernel

i.MX Yocto Project: How can I patch the kernel?

i.MX Yocto Project: How can I compile the kernel manually?

i.MX Yocto Project: Frequently Asked Questions

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信