Does i.MX534 compatible with i.MX535?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does i.MX534 compatible with i.MX535?

ソリューションへジャンプ
783件の閲覧回数
YanjunLuo
Contributor IV

Hi,

My i.MX535 board works fine, but I want it works under industrial environment, that is the temperature range is from -40C to +85C. Can I just solder i.MX534 on it? My design is based on i.MX53 Quick Start board with MC34708.

Regards,

Yanjun Luo.

ラベル(1)
0 件の賞賛
返信
1 解決策
707件の閲覧回数
Yuri
NXP Employee
NXP Employee

Most parts of i.MX53 series are pin compatible as much as they

have the same package (19 x 19 mm, 0.8 mm pitch BGA) and support

the same set of internal modules.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
708件の閲覧回数
Yuri
NXP Employee
NXP Employee

Most parts of i.MX53 series are pin compatible as much as they

have the same package (19 x 19 mm, 0.8 mm pitch BGA) and support

the same set of internal modules.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
707件の閲覧回数
YanjunLuo
Contributor IV

Hi Yuri,

Thank you for your information.

Regards,

Yanjun Luo.

0 件の賞賛
返信