Does i.MX534 compatible with i.MX535?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does i.MX534 compatible with i.MX535?

Jump to solution
671 Views
YanjunLuo
Contributor IV

Hi,

My i.MX535 board works fine, but I want it works under industrial environment, that is the temperature range is from -40C to +85C. Can I just solder i.MX534 on it? My design is based on i.MX53 Quick Start board with MC34708.

Regards,

Yanjun Luo.

Labels (1)
0 Kudos
Reply
1 Solution
595 Views
Yuri
NXP Employee
NXP Employee

Most parts of i.MX53 series are pin compatible as much as they

have the same package (19 x 19 mm, 0.8 mm pitch BGA) and support

the same set of internal modules.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
596 Views
Yuri
NXP Employee
NXP Employee

Most parts of i.MX53 series are pin compatible as much as they

have the same package (19 x 19 mm, 0.8 mm pitch BGA) and support

the same set of internal modules.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
595 Views
YanjunLuo
Contributor IV

Hi Yuri,

Thank you for your information.

Regards,

Yanjun Luo.

0 Kudos
Reply