Data transfer between external controller to IMX8QM-MEK through SPI or UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Data transfer between external controller to IMX8QM-MEK through SPI or UART

ソリューションへジャンプ
1,764件の閲覧回数
vinothkumars
Senior Contributor IV

Hi All,

 

I have a Companion microcontroller which is already flashed with RTOS and this Controller continuosly transfer the data over SPI or UART.

I needs to get the data to the linux (IMX8QM A9 Processor). Is there any way to get to it. or it should be simlar like normal UART or SPI interface

 

 

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
1 解決策
1,754件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

>I needs to get the data to the linux (IMX8QM A9 Processor). Is there any

>way to get to it. or it should be simlar like normal UART or SPI interface

 

yes, for uart,spi one can use standard linux APIs as described in  i.MX Linux Reference Manual​

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,755件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

>I needs to get the data to the linux (IMX8QM A9 Processor). Is there any

>way to get to it. or it should be simlar like normal UART or SPI interface

 

yes, for uart,spi one can use standard linux APIs as described in  i.MX Linux Reference Manual​

 

Best regards
igor

0 件の賞賛
返信