DDR clk value

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR clk value

676件の閲覧回数
dhanunjay
Contributor III

HI All,

I want to change imx6 DL DDR clk frequency to 410MHz, is it possible? can you pl. give example bare-metal ?

Is it possible to change DDR clk frequency run time?

ラベル(3)
0 件の賞賛
返信
1 返信

549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DHANUNJAY

it can be changed running code from iRAM for changing system PLL,

check sect.18.5.1.3.3 System PLL, sect.18.5.1.5.3 PLL clock change

i.MX6DQ Reference Manual: http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf.

In runtime the same procedure can be used. For example bare-metal please

create service request.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信