DDR clk value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR clk value

595 Views
dhanunjay
Contributor III

HI All,

I want to change imx6 DL DDR clk frequency to 410MHz, is it possible? can you pl. give example bare-metal ?

Is it possible to change DDR clk frequency run time?

Labels (3)
0 Kudos
Reply
1 Reply

468 Views
igorpadykov
NXP Employee
NXP Employee

Hi DHANUNJAY

it can be changed running code from iRAM for changing system PLL,

check sect.18.5.1.3.3 System PLL, sect.18.5.1.5.3 PLL clock change

i.MX6DQ Reference Manual: http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf.

In runtime the same procedure can be used. For example bare-metal please

create service request.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply