I have the cross_compile is arm-linux-gnueabihf4.7. Now i use for LTIB to cross_compile ubuntu 12.04, now there is two error.
FIRST,when i carry on sudo ./ltib -c,
the error is :
+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ oldconfig
scripts/kconfig/conf --oldconfig Kconfig
#
# configuration written to .config
#
+ [ -f /home/znzx/Desktop/ltib/config/platform/imx/imx6_defconfig.dev ]
+ diff -q ./.config /home/znzx/Desktop/ltib/config/platform/imx/imx6_defconfig.dev
+ [ -n ]
+ grep -q VERSION = 2 Makefile
+ [ %{kernel_series} = 2.4 ]
+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ uImage
scripts/kconfig/conf --silentoldconfig Kconfig
CHK include/linux/version.h
CHK include/generated/utsrelease.h
make[1]: `include/generated/mach-types.h' is up to date.
CC kernel/bounds.s
arm-linux-gnueabihf-gcc: error: -mfloat-abi=soft and -mfloat-abi=hard may not be used together
make[1]: *** [kernel/bounds.s] Error 1
make: *** [prepare0] Error 2
make: *** Waiting for unfinished jobs....
CC scripts/mod/empty.o
arm-linux-gnueabihf-gcc: error: -mfloat-abi=soft and -mfloat-abi=hard may not be used together
make[2]: *** [scripts/mod/empty.o] Error 1
make[1]: *** [scripts/mod] Error 2
make[1]: *** Waiting for unfinished jobs....
make: *** [scripts] Error 2
error: Bad exit status from /home/znzx/Desktop/ltib/tmp/rpm-tmp.39089 (%build)
RPM build errors:
Bad exit status from /home/znzx/Desktop/ltib/tmp/rpm-tmp.39089 (%build)
Build time for kernel-3.0.35: 10 seconds
Failed building kernel-3.0.35
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Fri Apr 17 14:54:31 2015
Ended: Fri Apr 17 14:55:25 2015
Elapsed: 54 seconds
These packages failed to build:
kernel-3.0.35
Build Failed
when i cross_compile without build uboot and kernel .
there is another error:
+ [ -n ]
+ [ -f /home/znzx/Desktop/ltib/config/.config ]
+ cat /home/znzx/Desktop/ltib/config/.config
+ perl -ne print if m,^CONFIG_(?!PCF),
+ [ ! -f config/platform/imx/.config -a -f config/platform/imx/defconfig ]
+ [ -n ]
+ cd config/platform/imx
+ mconf main.lkc .config
*** End of configuration.
*** Check the top-level Makefile for additional configuration options.
+ cp .config defconfig.dev
Processing platform: Freescale iMX6x Based Boards
===================================================
using config/platform/imx/.config
Processing: fake-provides
===========================
Processing: skell
===================
Processing: base_libs
=======================
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/znzx/Desktop/ltib/rootfs --dbpath /var/lib/rpm -e --allmatches --nodeps --define '_tmppath /tmp/ltib' base_libs 2>/dev/null
sudo /opt/freescale/ltib/usr/bin/rpm --root /home/znzx/Desktop/ltib/rootfs --dbpath /var/lib/rpm --prefix / --ignorearch -ivh --force --excludedocs --define '_tmppath /tmp/ltib' /home/znzx/Desktop/ltib/rpm/RPMS/arm/base_libs-1.2-1.arm.rpm
error: failed dependencies:
ld-linux.so.3(GLIBC_2.4) is needed by base_libs-1.2-1
f_buildrpms() returned an error, exiting
traceback:
main:572
Started: Fri Apr 17 14:56:45 2015
Ended: Fri Apr 17 14:56:59 2015
Elapsed: 14 seconds
Build Failed
Exiting on error or interrupt
znzx@ubuntu:~/Desktop/ltib$
someone can give some suggests?
according to the error message: "arm-linux-gnueabihf-gcc: error: -mfloat-abi=soft and -mfloat-abi=hard may not be used together"
You are using both 'soft' and 'hard' floating point setting.
So you may use "-mfloat-abi=hard" only in the LTIB configuration. By default, the toolchain is using gcc-4.6.2. If you use a different compiler, you may need a new toolchain.
i get a new toolchain where is gcchf-4.7.while carry on the ./ltib -c ,it occur a problem like the arm-linux-gnueabihf-gcc: error: -mfloat-abi=soft and -mfloat-abi=hard may not be used togethe.
when i compile without kernel ,the promble whichi is ld-linux.so.3(GLIBC_2.4) is needed by base_libs-1.2-1
Have you try -distclean first? or remove everything in rpm/BUILD/ ?
I tried to use the default toolchain gcc-4.6.2 with -mfloat-abi=hard. The build is fine without error.
yeah,when i follow the instruction without error, while when i instead of the compile ,the error is coming.
there is not person meet this question?