Connecting a 7 inch display to iMXRT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting a 7 inch display to iMXRT1060

1,720 Views
EmbeddedTech
Contributor III

Hi,

We would like to connect a 7 inch LCD to the iMXRT1060 EVK board. Is there any evaluation board already available with 7 inch display?

Also in the application note below,

https://www.nxp.com/docs/en/application-note/AN12302.pdf

There is a reference to LCD extension board. Is this board for interfacing the 7" LCD with the EVK?

How to order this extension board?

Your help on this is highly appreciated.

Thanks.

Labels (1)
0 Kudos
Reply
6 Replies

1,699 Views
EmbeddedTech
Contributor III

Hi,

 

May I know what LCD part is used in the application note AN12302.pdf?

Is it a 7 inch or 10 inch LCD?

Will that LCD work directly on connecting to the LCD interface (if using RGB 565 mode) on the EVK or it requires hardware changes?

If connecting to LVDS, what changes need to be done in the hardware on EVK?

Thanks.

 

0 Kudos
Reply

1,692 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) May I know what LCD part is used in the application note AN12302.pdf?
-- Please check the attachment.
2) Is it a 7 inch or 10 inch LCD?
-- 10 inch.
3) If connecting to LVDS, what changes need to be done in the hardware on EVK?
-- The LCD module actually doesn't support the LVDS interfacer.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,690 Views
EmbeddedTech
Contributor III

Hi,

Thanks for the datasheet.

Is it possible and is it recommended to use LVDS display on iMXRT1060 by using a RGB to LVDS converter? 

Thanks.

0 Kudos
Reply

1,687 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is it possible and is it recommended to use LVDS display on iMXRT1060 by using an RGB to LVDS converter?
-- Yes, I think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,709 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there any evaluation board already available with 7 inch display?
-- No。
2) Is this board for interfacing the 7" LCD with the EVK?
-- The MIMXRT1060 EVK board is able to interface a 7" LCD panel.
3) How to order this extension board?
-- LCD extension board is created by the AE team for testing, it's not for sales.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,706 Views
EmbeddedTech
Contributor III

Thanks for your reply.

0 Kudos
Reply