Connecting a 7 inch display to iMXRT1060

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Connecting a 7 inch display to iMXRT1060

1,723 次查看
EmbeddedTech
Contributor III

Hi,

We would like to connect a 7 inch LCD to the iMXRT1060 EVK board. Is there any evaluation board already available with 7 inch display?

Also in the application note below,

https://www.nxp.com/docs/en/application-note/AN12302.pdf

There is a reference to LCD extension board. Is this board for interfacing the 7" LCD with the EVK?

How to order this extension board?

Your help on this is highly appreciated.

Thanks.

标签 (1)
0 项奖励
回复
6 回复数

1,702 次查看
EmbeddedTech
Contributor III

Hi,

 

May I know what LCD part is used in the application note AN12302.pdf?

Is it a 7 inch or 10 inch LCD?

Will that LCD work directly on connecting to the LCD interface (if using RGB 565 mode) on the EVK or it requires hardware changes?

If connecting to LVDS, what changes need to be done in the hardware on EVK?

Thanks.

 

0 项奖励
回复

1,695 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) May I know what LCD part is used in the application note AN12302.pdf?
-- Please check the attachment.
2) Is it a 7 inch or 10 inch LCD?
-- 10 inch.
3) If connecting to LVDS, what changes need to be done in the hardware on EVK?
-- The LCD module actually doesn't support the LVDS interfacer.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,693 次查看
EmbeddedTech
Contributor III

Hi,

Thanks for the datasheet.

Is it possible and is it recommended to use LVDS display on iMXRT1060 by using a RGB to LVDS converter? 

Thanks.

0 项奖励
回复

1,690 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is it possible and is it recommended to use LVDS display on iMXRT1060 by using an RGB to LVDS converter?
-- Yes, I think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,712 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there any evaluation board already available with 7 inch display?
-- No。
2) Is this board for interfacing the 7" LCD with the EVK?
-- The MIMXRT1060 EVK board is able to interface a 7" LCD panel.
3) How to order this extension board?
-- LCD extension board is created by the AE team for testing, it's not for sales.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,709 次查看
EmbeddedTech
Contributor III

Thanks for your reply.

0 项奖励
回复