I am trying to connect 2 sabre lite iMx6 Quad boards (from boundary devices) over Ethernet.
Both boards run Android Lollipop.
If I connect them via an Ethernet Switch, the lights on the Ethernet connectors light up and blink. I can also ping from one board to the other. I also can open a TCP/IP socket and send data back and forth.
When I connect the 2 boards directly to each other using a cross over ethernet cable, the lights do not blink and I cannot ping from one board to another.
Has anybody tried this before?
Do you have any suggestions to solve this issue?
Please make sure that IP is configured respectively.
I mean both boards have static IP addresses in the same network.
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Victor,
Yes, I have configured both boards to have static IP addresses (192.168.1.2 and 192.168.1.3)
David
Also please make sure that you are using right cable.
I mean you need to use crossover cable when you are connecting the devices directly (without a switch).
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David,
do you configured IP addresses of each board?
Michal