Hi All,
I'm trying to add self-refresh mode support for lpddr2 on imx6sll. I was able to establish an approximate list of "mmdc" registers,
static const u32 imx6sll_mmdc_lpddr2_offset[] __initconst = {
0x01c, 0x800, 0x85c, 0x890, /*MDSCR,MPZQHWCTRL,MPZQLP2CTL,MPPDCMPR2*/
0x8b8, 0x81c, 0x820, 0x824, /*MPMUR0,MPRDDQBY0DL,MPRDDQBY1DL,MPRDDQBY2DL*/
0x828, 0x82c, 0x830, 0x834, /*MPRDDQBY3DL,MPWRDQBY0DL,MPWRDQBY1DL,MPWRDQBY2DL*/
0x838, 0x83c, 0x848, 0x850, /*MPWRDQBY3DL,MPDGCTRL0,MPRDDLCTL,MPWRDLCTL*/
0x8c0, 0x8b8, 0x004, 0x00c, /*MPDCCR,MPMUR0,MDPDC,MDCFG0*/
0x010, 0x038, 0x014, 0x018, /*MDCFG1,MDCFG3LP,MDCFG2,MDMISC*/
0x01c, 0x02c, 0x030, /*MDSCR,MDRWD,MDOR*/
0x040, 0x000, 0x020, /*MDASP,MDCTL,MDREF*/
0x800, 0x004, 0x01c, /*MPZQHWCTRL,MDPDC,MDSCR*/
};
thanks to a reference manual, and values for some of them,
pm_info->mmdc_val[0][1] = 0x8000;
pm_info->mmdc_val[1][1] = 0xa1390003;
pm_info->mmdc_val[3][1] = 0x400000;
pm_info->mmdc_val[4][1] = 0x800;
pm_info->mmdc_val[17][1] = 0x800;
pm_info->mmdc_val[18][1] = 0x20024;
pm_info->mmdc_val[23][1] = 0x201708;
pm_info->mmdc_val[24][1] = 0x8000;
pm_info->mmdc_val[30][1] = 0xa1310003;
but I can not find any information about the list of "mmdc io" registers for imx6sll. All this is complicated by the fact that in imx6sll there are no "mmdc io" registers (CAS, RAS, SODT0, SODT1, DRAM_RESET), and because of this I can not make simple mapping of registers from another processor, such as imx6sl or imx6sx.
Can anyone tell me which "mmdc io" registers I need to save, or is it possible for someone to have documentation on this topic for imx6sll?
Thanks & Regards,
Valentin