Configuring imx6 USB OTG port as USB Host by default

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configuring imx6 USB OTG port as USB Host by default

5,527 次查看
karthigeyannata
Contributor III

We would like to configure imx6 USB OTG port in USB Host mode by default. We have not used USB OTG ID pin in our HW.

Could you please advise the SW changes required to do the same?

标签 (1)
0 项奖励
回复
2 回复数

955 次查看
SergioSolis
NXP Employee
NXP Employee


Please take a look at this post and check if it helps you:

IMX53 USB OTG Host mode.


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

955 次查看
karthigeyannata
Contributor III

After the device is connected when the imx6 is in Host mode,  we would like to do role switch in the software to make imx6 to work in device mode.

is this possible with above mentioned procedure?

0 项奖励
回复