Hi all
I'm using i.MX6Solo and have a question about ERR005198.
I can't understand the conditions of PL310 internal access request.
According to the errata, there are following description.
I understand the information will be sampled when PL310 requested.
This information is associated with each individual RAM access, and is only meant to be sampled
by the PL310 internal access requestor at precise cycles, depending on the programmable latencies
of the accessed RAM.
What situation will make the PL310 internal access request ?
Ko-hey
已解决! 转到解答。
There is so-called Internal instruction and data prefetch engine within the L2 cache controller that periodically generates internal accesses to the L2 cache RAM. For more information, please refer to the corresponding ARM document:
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0246h/DDI0246H_l2c310_r3p3_trm.pdf
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
There is so-called Internal instruction and data prefetch engine within the L2 cache controller that periodically generates internal accesses to the L2 cache RAM. For more information, please refer to the corresponding ARM document:
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0246h/DDI0246H_l2c310_r3p3_trm.pdf
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------