Conditions of PL310 internal access request

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Conditions of PL310 internal access request

ソリューションへジャンプ
1,649件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I'm using i.MX6Solo and have a question about ERR005198.

I can't understand the conditions of PL310 internal access request.

According to the errata, there are following description.

I understand the information will be sampled when PL310 requested.

This information is associated with each individual RAM access, and is only meant to be sampled

by the PL310 internal access requestor at precise cycles, depending on the programmable latencies

of the accessed RAM.

What situation will make the PL310 internal access request ?

Ko-hey

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,408件の閲覧回数
art
NXP Employee
NXP Employee

There is so-called Internal instruction and data prefetch engine within the L2 cache controller that periodically generates internal accesses to the L2 cache RAM. For more information, please refer to the corresponding ARM document:

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0246h/DDI0246H_l2c310_r3p3_trm.pdf


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,409件の閲覧回数
art
NXP Employee
NXP Employee

There is so-called Internal instruction and data prefetch engine within the L2 cache controller that periodically generates internal accesses to the L2 cache RAM. For more information, please refer to the corresponding ARM document:

http://infocenter.arm.com/help/topic/com.arm.doc.ddi0246h/DDI0246H_l2c310_r3p3_trm.pdf


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,408件の閲覧回数
ko-hey
Senior Contributor II

Hi Artur

Thank you for reply.

Do you mean that there are no particular conditions that PL310 internal access are requested ?

ko-hey

0 件の賞賛
返信
1,408件の閲覧回数
art
NXP Employee
NXP Employee

The details of the internal prefetch engine operation are described in the document I' ve pointed to you laast time.

Best Regards,

Artur

0 件の賞賛
返信