I'm developing an application in Qt on imx6Solox. I created the image with Wayland and its kernel version is 4.15.2.1.0. I'm wondering how to change the Nxp logo while is shown the system is booting. Also, can I upload a video in splash screen? If yes, how? Finally, I want to make my own distro or OS for imx, how can I make this? Could you suggest me a book or an article to make these?
解決済! 解決策の投稿を見る。
ycoto splash screen is a recipe, you can rebuild rootfs in yocto's way, or make it manual.
ootput file psplash and psplash-write is in rootfs's /usr/bin/ dir.
Hi Bharghavi K,
What you see in the above pic is Plash Screen not Boot logo,Then you need change the Plash Screen,please do the following steps :
convert yourimage.* to yourimage.h, then follow below steps,
1) copy the myimage.h to ../../../sources/poky/meta-yocto/recipes-core/psplash/files/myimage.h.
2) MACHINE=your-machine-name source fsl-setup-release.sh –b build –e fb.
3) bitbake your-image-name.
BR
Nandish SG
Hi nandish,
Thank u,I converted the image .* to myimage.h.Copied to fsl-community-bsp/sources/poky/meta-yocto/recipes-core/psplash/files/
While executing ->MACHINE=wandboard source fsl-setup-release.sh -b build -e fb
I'm getting as like below mentioned.
bash: fsl-setup-release.sh: No such file or directory.
How can i solve this issue?
Thanks in advance.
Hi Bhargavi K,
Step1:
First you need to change the image format from ( * = your image name)
a) *.png to *.pnm
b) *.pnm to *ppm
Step2:
Replace the your converted *.ppm file with original *.ppm file in .../git/driver/video/logo/*.ppm
Step3:
Recompile your zImage or uImage or Image (The one which Image you are using for your board). by using your Cross Compiler, Now Task is done and re-flash the image to your SD-card,
I hope i am clear with this, after done this task if not please let me know ,
Best Regards,
Nandish SG
Hi nandish gurulingappa,
I tried the above u suggested steps.After power on the my wandboardboard-quad it is displaying wandboard.org logo not displaying my logo.I followed steps as mentioned below is any wrong please let me know.My actual image is below mentioned.
Converted .png to .pnm and .pnm to .ppm
step-1.
-->pngtopnm whileboot.png > linuxlogo.pnm
-->pnmquant 224 linuxlogo.pnm > linuxlogo224.pnm
-->pnmtoplainpnm linuxlogo224.pnm > linuxlogo224.ppm
step-2.
Later moved the linuxlogo224.ppm file to build/tmp/work/wandboard_quad-poky-linux-gnueabi/linux-wandboard/3.10.17-r0/git/drivers/video/logo replaced it as logo_linux_clut224.ppm
step-3.
Compiled the image
-->bitbake core-image-minimal
The image flashed to sdcard by below command
-->sudo dd if=tmp/deploy/images/wandboard-quad/core-image-minimal-wandboard-quad.sdcard of=/dev/sdb bs=4M && sudo sync
And finally verified on my target board its not displayed my logo.What is the issue?Please let me know.
Thanks and Regards.
Hi Bharghavi K,
What you see in the above pic is Plash Screen not Boot logo,Then you need change the Plash Screen,please do the following steps :
convert yourimage.* to yourimage.h, then follow below steps,
1) copy the myimage.h to ../../../sources/poky/meta-yocto/recipes-core/psplash/files/myimage.h.
2) MACHINE=your-machine-name source fsl-setup-release.sh –b build –e fb.
3) bitbake your-image-name.
BR
Nandish SG
Hi kk d,
apologize for late reply, Based on your quires my solutions is below,
I hope you know how to convert yourimage.* to yourimage.h, then follow below steps,
1) copy the myimage.h to ../../../sources/poky/meta-yocto/recipes-core/psplash/files/myimage.h.
2) MACHINE=your-machine-name source fsl-setup-release.sh –b build –e fb.
3) bitbake your-image-name.
Best Regards,
Nandish SG
I followed your steps as u mentioned above.
I converted myimage1.png image to myimage1.h file and I replaced image.h(imx6 logo) with myimage1.h file. and it successfully displayed on splash screen. for this image bitbake runs around 30 tasks outof 7024.
But when I tried with some other image say myimage2.h its still showing previous image myimage1.h for this image bitbake runs 0 tasks. I think problem is with bitbake and also I tried following commads
"bitbake psplash -c cleansstate"
"bitbake psplash"
and also "bitbake -c cleansstate"
Still no luck. Do you have any idea?
Thanks in advance
SubbaReddy GV
Hi SubbaReddy Garu,
You need to clean the all obj file which were generated during compilation ,Please try with the below commands,
1) ./setup-environment build (build = your directory name for where the source code present)
2) bitbake -c cleansstate linux-imx
3) bitbake
after this copy the image to sd card and please let me know,
Best Regards,
Nandish S.G
Hi Nandish,
I run "bitabake -c cleansstate linux-esomimx6" image successfully changed again when I tried with other image its not flashing on screen.
Thank you
SubbaReddy GV
Hi,
I Converted .png image to .ppm and copied to this location /usr/src/linux-headers-3.13.0-24/drivers/video/logo/logo_linux_clut224.ppm
I converted .png image to myimage.h and copied to ../sources/poky/meta-yocto/recipes-core/psplash/files/myimage.h.
MACHINE=wandboard-quad and source fsl-setup-release.sh -b build -e fb.After executing the source setup i got no such file or directory below mentioned.
bash: fsl-setup-release.sh: No such file or directory.
I tried with . ./setupenvironment build, bitbake core-image-minimal.
Copied to sdcard and verified in my wandboard-quad,its not displaying my logo.Can you please tell me where the issue is and suggest me how to solve the issue.
Thanks and Regards.
Hi nandish,
I tried the above steps u suggested.I'm not able to get my logo,its displaying wandboard logo.
I found in this path wandboard logo is present build/tmp/work/wandboard_quad-poky-linux-gnueabi/u-boot-fslc/v2014.10+gitAUTOINC+5fd0b607d0-r0/git/tools/logos.
The logo is .bmp
After flashing sdcard and placed in wandboard-quad its displaying above logo.How to find in sdcard logos are presented?
Thanks in advance
Hello Bhargavi K,
The above steps build your image right ?,
Then you need to change the logo file .i.e
Step1:
First you need to change the image format from ( * = your image name)
first change the .bmp file to .png file then do below steps.
-->pngtopnm linuxlogo.png > linuxlogo.pnm
-->pnmquant 224 linuxlogo.pnm > linuxlogo224.pnm
-->pnmtoplainpnm linuxlogo224.pnm > linuxlogo224.ppm
Step2:
Replace the your converted *.ppm file with original *.ppm file in build/tmp/work/wandboard_quad-poky-linux-gnueabi/u-boot-fslc/v2014.10gitAUTOINC5fd0b607d0-r0/git/tools/logos.
Step 3:
Recompile your Image,
After doing the above steps please let me know.
BR
Nandish SG
nandish gurulingappa wrote:
Hello Bhargavi K,
The above steps build your image right ?,
Then you need to change the logo file .i.e
Step1:
First you need to change the image format from ( * = your image name)
first change the .bmp file to .png file then do below steps.
-->pngtopnm linuxlogo.png > linuxlogo.pnm
-->pnmquant 224 linuxlogo.pnm > linuxlogo224.pnm
-->pnmtoplainpnm linuxlogo224.pnm > linuxlogo224.ppm
Step2:
Replace the your converted *.ppm file with original *.ppm file in build/tmp/work/wandboard_quad-poky-linux-gnueabi/u-boot-fslc/v2014.10gitAUTOINC5fd0b607d0-r0/git/tools/logos.
Step 3:
Recompile your Image,
After doing the above steps please let me know.
BR
Nandish SG
The above builded image is right.I changed the logo file .bmp to ppm as per u suggested.Converted .ppm logo replaced in above given path.Still persist same logo,not able to display mylogo.I'm getting wandboardlogo.
I want to display the yocto project logo below mentioned in attachment .I attached screen shot of the ppm and bmp images.Please find the attachments and let me know where is the issue?
Hi Nandish,
Thanks for replying.I found the PPM file is in build/tmp/work/wandboard_quad-poky-linux-gnueabi/linux-wandboard/3.10.17-r0/git/drivers/video/logo.Still i didn't solved my issue.Please suggest me the procedure for changing logo on wandboard-quad using yocto.
Thanks in advance
Bhargavi K
Hello Nandish,
The path for wandboard.org image is build/tmp/work/wandboard_quad-poky-linux-gnueabi/u-boot-fslc/v2014.10gitAUTOINC5fd0b607d0-r0/git/tools/logos.But in that path all images are .bmp none of the image are .ppm. As mentioned in above attached screenshot file.I removed the wandboard logo in that path.After recompiling same image it is displaying on wandboard-quad.I want to get to know the image already deleted but how it is displaying ?or i have to check in sdcard while placing on wandboard-quad?
Thanks and Regards