Dear Community,
I would like to know if it is possible to use the iMX6Q (or some alternative) for capturing the 16-bit YUV data output from the THC63LVD1024 converter which converts LVDS signal from the Sony FCB-EV9520L camera.
I saw similar questions but without solutions, however :
https://community.nxp.com/t5/i-MX-Processors/Could-not-configure-CSI0-bt-1120-on-i-MX6Q/m-p/750813
https://community.nxp.com/t5/i-MX-Processors/imx6q-ipu2-csi-2-16-bit-yuv-video/m-p/898111
Thanks in advance and best regards,
Khang
do you mind sharing more detailed information? the link you attach is about BT1120, if you just use yuv 16bits, imx6q can support it, and how you connect your camera? mipi csi port or parallel port?
Hi @joanxie,
The camera manufacturer confirmed that its output is compliant with BT709 :
And we plan to connect the camera to the iMX6Q via the THC63LVD1024 to convert LVDS signals to LVCMOS parallel.
Best Regards,
Khang