Hi i.MX8 EVM Experts,
Now I'm trying to prepara reference debug environmnt of i.MX8 LCD output (LVDS).
My developping provide will use LCD panel of 1280x480 size, connect via LVDS .
And to check the SW behavior, now I'm consider to use i.MX8 EVM plus IMX-LVDS-HDMI board, and connect it to ordinally 1920x1080 PC monitor.
1. does IMX-LVDS-HDMI can convert LVDS 1280 x 480 (or any other fllexible) resolutin output to HDMI ?
2. and if above 1. is yes, how the image will be appeared on Monitor ? i.e. will it diaplayed at adjested at left top corner, and remained area as blank ? or any resizing will be done to fit the PC monitor ersolution ?
thank in advance !
1. does IMX-LVDS-HDMI can convert LVDS 1280 x 480 (or any other fllexible) resolutin output to HDMI ?
=> For the information related to supported resolution, kindly refer to section 2.10 LVDS connectors (J15, J16) from the i.MX 8M Plus LPDDR4 EVK Board Hardware User's Guide