Can't boot Android from SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't boot Android from SD

1,244 次查看
dmitriipetrov
Contributor I

Log from u boot says:

mmc1 is current device                                                    
** Unrecognized filesystem type **                                        

** Unrecognized filesystem type **

I have made SD card from prebuilt images (android_L5.0.0_1.0.0-ga_images_6qsabreauto.tar.gz)

Any help?

标签 (2)
0 项奖励
回复
2 回复数

1,117 次查看
SergioSolis
NXP Employee
NXP Employee

How did you perform the flashing?, did you do it manually or used manufacturing tool?

0 项奖励
回复

1,117 次查看
dmitriipetrov
Contributor I

I have done it manually, because i have now only Ubuntu on my PC.

dmitrii@dmitrii-Predator-G3-605:~/test/android_5_freescale/image_to_flash$ sudo dd if=u-boot-imx6qsabreauto_sd.imx of=/dev/sdb bs=1K seek=1; sync

407+0 records in

407+0 records out

416768 bytes (417 kB) copied, 0,816086 s, 511 kB/s

dmitrii@dmitrii-Predator-G3-605:~/test/android_5_freescale/image_to_flash$ sudo dd if=boot-imx6q.img of=/dev/sdb1; sync

14844+1 records in

14844+1 records out

7600384 bytes (7,6 MB) copied, 1,79037 s, 4,2 MB/s

dmitrii@dmitrii-Predator-G3-605:~/test/android_5_freescale/image_to_flash$ sudo dd if=system.img of=/dev/sdb5; sync

737240+0 records in

737240+0 records out

377466880 bytes (377 MB) copied, 38,9548 s, 9,7 MB/s

dmitrii@dmitrii-Predator-G3-605:~/test/android_5_freescale/image_to_flash$ sudo dd if=recovery.img of=/dev/sdb2; sync

15916+1 records in

15916+1 records out

8149248 bytes (8,1 MB) copied, 2,66373 s, 3,1 MB/s

0 项奖励
回复