Can not force IDR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not force IDR

1,336件の閲覧回数
marko1921
Contributor I

Hello. I'm playing with encode_stream.c and test_enc_arm_elinux.c in imx-vpuwrap repository

VPU wrapper version is

vpu lib version : major.minor.rel=1.1.1
vpu fw version : major.minor.rel_rcode=1.1.1_r0
vpu wrapper version : major.minor.rel=3.0.0: VPUWRAPPER_ARM64_LINUX

I'm receiving regular P-frame hen I'm trying to force IDR by setting field  sEncEncParam.nForceIPicture = 1.

How do I correctly force IDR ?

0 件の賞賛
返信
1 返信

1,316件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

When inserting a new IDR frame, drain your pipeline and reset.  There are only a few changes that are completely safe to do without a drain/reset.  Use mfxExtEncoderResetOption=ON to make sure that a new sequence is started.

To ensure that mfxEncodeCtrl parameters correctly correspond to intended frame, allocate as many of them as surfaces used by the encoder. 

Regards

0 件の賞賛
返信