Can i.MX8M mini use DDR3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX8M mini use DDR3?

5,757 Views
danny_kim
Contributor III

Hi 

I purchased i.MX8M mini EVK
The EVK I purchased has 2GB of LPDDR4 designed.
(There are also EVKs designed with DDR4)


Can I change to  DDR3?
Can I design with 512MB or 1GB?

The product I am designing now does not have much work on the video side.
It is about checking the video seamlessly by connecting HD-class CAM with USB.

Please review
Thank you

Labels (2)
21 Replies

5,343 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

i.MX8 Mini supports 32/16-bit LPDDR4 (up to 1.5 GHz), DDR4-2400, and DDR3L-1600. It also supports up to 8 Gbyte DDR memory space.

Regards,

Mrudang

5,343 Views
danny_kim
Contributor III

Hi Mrudang

DDRL can be used. Can I modify it by referring to the DDR4 design?
Please share any information I can refer to.

And is there no problem with 1GB or 512MB other than 2GB?

Thank you

0 Kudos
Reply

5,343 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

Yes DDR3L can be used. And there is no issue with 1GB or 512MB.

Kindly share your schematic once you are done with the interfacing.

Mrudang

5,342 Views
danny_kim
Contributor III

Hi Mrudang

I designed schematic a part of i.MX8, DDR3L, eMMC

Please review my schematic

Thank you

0 Kudos
Reply

5,341 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

Please refer to IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide for DDR3L.

  • Refer complete sec 3.4 DDR design recommendations for pin signal assignment, signal swapping etc.
  • Also, refer to reference schematic pg. no 5 of SCH-35104 for DDR3L interface and net swapping based on signal routing.
  • eMMC interface looks good. (Reference pg. no 9 of SCH-31399 C2)

Regards,

Mrudang

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

I will refer to IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide

But I have a question
Where is the circuit diagram for reference (SCH-35104, SCH-31399)?
This is not in IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide, what document?
Is the document I know different from the document you are telling me?
Please let me know

Thank you

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

Please find the attached schematic for your reference.

Regards,

Mrudang

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

The attached file is a circuit diagram for LPDDR4 and DDR4
Is there any circuit diagram for DDR3L?

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

The schematic is based on DDR4 and LPDDR4. but they have also mentioned DDR3 as well. It means this reference schematic is also applicable for DDR3 signal interface as well.

pastedImage_2.png

Section 3.4 of  IMX8MMHDG: i.MX 8M Mini Hardware Developer’s Guide has provided pin signal assignment for all 3 DRAM.

Mrudang

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

I referred to the document composed of DDR4 (SPF-35104) and prepared a circuit diagram for review. (The circuit diagram was attached)
Have you seen the circuit diagram I attached?
If you have seen it, please give me a comment on it

According to the document (IMX8MMHDG: i.MX 8M Mini Hardware Developer's Guide), when using DDR3L, it seems to use four DDR3L.
However, the circuit diagram using DDR4 uses two DDR4.
If there is a circuit diagram composed of DDR3L, please attach it.
Thanks

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

Please resend me the updated schematic.

If they have used 4 DRAM for their application. If we need to use 2 DRAM based on data lines and memory density we need to connect the DQ signals and address signals.

Mrudang.

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

Among the above ripples, there is a circuit diagram I attached
I want you to give me a comment on it

1. Only two DDR3Ls are used? Should I use 4?
2. Please inform the wrong part of the attached circuit diagram.
3. Please attach a reference circuit diagram written in DDR3L.
4. Is there a circuit diagram written in i.MX8MM and DDR3L?

Thank you

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

The attachment is missing.

Please share the updated one.

What do you mean by the wrong part?

Do you use Skype?

Share your id.

Mrudang

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

Attached file is here

pastedImage_1.png

'Wrong part' is to review the circuit diagram
I'm sorry, but I don't use Skype
Is there no DDR3L circuit diagram?

Thank you

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Hi Danny,

As I have informed you earlier, pls assign the data lines as shown in ref design.

pastedImage_1.png

pastedImage_2.png

Please update.

Mrudang

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

I modified the data line and attached circuit
Is there anything else that could be a big problem besides the data line?

I think the wiring of DDR4 and DDR3L is similar, so I can do artwork by referring to the DDR4 schematic and PCB file.

Thank you

 

0 Kudos
Reply

5,341 Views
mrudangshelat1
Senior Contributor II

HI Danny,

Now DRAM looks good. I believe Parity, Ten and ACT_n pins are not there in DDR3L. Those are for DDR4.

Is there anything else that could be a big problem besides the data line?

Ans: Data Mask, Data strobe has to be matched with Data lines. Earlier schematic it was not matching.

I think the wiring of DDR4 and DDR3L is similar, so I can do artwork by referring to the DDR4 schematic and PCB file.

Ans: Yes.

Mrudang

5,340 Views
danny_kim
Contributor III

Hi Mrudang

I don't use it in DDR3L, but I will treat Parity, Ten and ACT-N as TP

The other part of the wiring of DDR3L is said to be okay, so I will start working as it is.
Thank you

0 Kudos
Reply

5,342 Views
mrudangshelat1
Senior Contributor II

Sure

0 Kudos
Reply

5,342 Views
danny_kim
Contributor III

Hi Mrudang

i.MX8M mini is applicable to DDR3L and 512MB is also available.
Then I will design DDR3L, 1GB
I'll share it when finished, so please review
Thank you

0 Kudos
Reply