Can i.MX25 be boot from NAND-Flash with 4 K byte-page?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX25 be boot from NAND-Flash with 4 K byte-page?

Jump to solution
1,708 Views
george
Senior Contributor II

Dear all,

We have decided to use i.MX25 to the next product.

It is the request from our end user.

And they request more that 2GB(16Gb) NAND-Flash is used.

I chose Micron's NAND-Flash (MT29F16G08ADBCAH4-IT).

The page size is 4320 bytes (4096 + 224 bytes) and it is not officially supported by i.MX25.

But, it is that use is possiblehere.

After all, can i.MX25 be booted from Code in MT29F16G08ADBCAH4-IT?

(by spare size to 218 and a few repeating reset)

Best Regards,

Fukutomi

Labels (5)
0 Kudos
Reply
1 Solution
1,374 Views
jamesbone
NXP TechSupport
NXP TechSupport

Dear George,

Your understanding is correct, the Linux kernel it is able to handle the 4K page of NAND flash, But the Boot Rom Code only supports 2K.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
1,374 Views
jamesbone
NXP TechSupport
NXP TechSupport

alejandrolozano,  Is the 4K page supported at boot?

1,374 Views
george
Senior Contributor II

Dear jamesbone,

Thank you for the response.

  a) Depending on the case, NAND-Flash which has 4K page can be used by linux-kernel.

  b) But, It cannot boot from NAND Flash which has 4K page.

Is my understanding correct?

BR,

George

0 Kudos
Reply
1,375 Views
jamesbone
NXP TechSupport
NXP TechSupport

Dear George,

Your understanding is correct, the Linux kernel it is able to handle the 4K page of NAND flash, But the Boot Rom Code only supports 2K.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,374 Views
fmvalero
Contributor II

Hi jamesbone,

Sorry, but I don't understand your answer. If you can't boot i.MX25 from a 4K page NAND, why can you select 4K page in the boot options (BT_PAGE_SIZE[1:0])? I have a similar post here and I was told that I shouldn't have problem.

Best regards,

Fernando.

0 Kudos
Reply
1,374 Views
george
Senior Contributor II

Dear jamesbone,

Thanks.

I understand.

BR,

George

0 Kudos
Reply