Hi,
I found that PCIE uses LVDS to transmit data.Can PCIE be used to receive LVDS data?
I want to use dp to lvds chip to convert the DP signal, and use the PCIE of MX6 to receive it. Is this feasible?
解決済! 解決策の投稿を見る。
yes, if custom driver will comply with protocols defined in PCIe specification.
Also HCSL logic is used for PCIe, description can be found for example in
https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en
Best regards
igor
Hi Simon
I am afraid it is not feasible, as i.MX6Q PCIe module works only with devices compatible with PCIe
specification : https://en.wikipedia.org/wiki/PCI_Express
also may be helpful
https://community.nxp.com/t5/i-MX-Processors/i-mx6Q-PCIe-clock/m-p/802364/highlight/true
Best regards
igor
Hi igor,
If I write my own LVDS driver, can I use MIPI-CSI or PCIE interface to receive LVDS?
Best regards
Simon
yes, if custom driver will comply with protocols defined in PCIe specification.
Also HCSL logic is used for PCIe, description can be found for example in
https://www.renesas.com/document/apn/808-pci-expresshcsl-termination?language=en
Best regards
igor