Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

1,455 次查看
yuvakrishna
Contributor II

Similar to Display and I2C, Is it possible to configure the Ethernet peripheral to the M4 in the IMX7D SOC? Is there any constrains such that only these specific peripherals can be configured via RDC?

As per my understanding this should also be feasible.

0 项奖励
回复
3 回复数

1,143 次查看
garyhubley
Contributor I

Has this been solved? Trying to determine the same thing myself.

0 项奖励
回复

1,188 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuva

yes it is possible, though I am not aware of such examples.

In general may be useful to look at FreeRTOS examples

 Board Support Packages (3)
FreeRTOS_iMX7D_1.0.1_LINUX(REV 1.0.1)
https://www.nxp.com/products/microcontrollers-and-processors/arm-based-processors-and-mcus/i.mx-appl...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,188 次查看
yuvakrishna
Contributor II

Also it would be great if any example is referenced.