Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

1,453 Views
yuvakrishna
Contributor II

Similar to Display and I2C, Is it possible to configure the Ethernet peripheral to the M4 in the IMX7D SOC? Is there any constrains such that only these specific peripherals can be configured via RDC?

As per my understanding this should also be feasible.

0 Kudos
Reply
3 Replies

1,141 Views
garyhubley
Contributor I

Has this been solved? Trying to determine the same thing myself.

0 Kudos
Reply

1,186 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuva

yes it is possible, though I am not aware of such examples.

In general may be useful to look at FreeRTOS examples

 Board Support Packages (3)
FreeRTOS_iMX7D_1.0.1_LINUX(REV 1.0.1)
https://www.nxp.com/products/microcontrollers-and-processors/arm-based-processors-and-mcus/i.mx-appl...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,186 Views
yuvakrishna
Contributor II

Also it would be great if any example is referenced.