Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can Ethernet Peripheral in IMX7 can be configured with M4 with help of RDC?

1,454件の閲覧回数
yuvakrishna
Contributor II

Similar to Display and I2C, Is it possible to configure the Ethernet peripheral to the M4 in the IMX7D SOC? Is there any constrains such that only these specific peripherals can be configured via RDC?

As per my understanding this should also be feasible.

0 件の賞賛
返信
3 返答(返信)

1,142件の閲覧回数
garyhubley
Contributor I

Has this been solved? Trying to determine the same thing myself.

0 件の賞賛
返信

1,187件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuva

yes it is possible, though I am not aware of such examples.

In general may be useful to look at FreeRTOS examples

 Board Support Packages (3)
FreeRTOS_iMX7D_1.0.1_LINUX(REV 1.0.1)
https://www.nxp.com/products/microcontrollers-and-processors/arm-based-processors-and-mcus/i.mx-appl...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,187件の閲覧回数
yuvakrishna
Contributor II

Also it would be great if any example is referenced.