i.MX6ULL NVCC_DRAM2P5 questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6ULL NVCC_DRAM2P5 questions

ソリューションへジャンプ
1,082件の閲覧回数
m_c
Senior Contributor I

1. Is NVCC_DRAM2P5 an input or output pin?

2. What is its role and how to use this pin?

3. Is it must connected with VDD_HIGH_CAP?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,033件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  NVCC_DRAM2P5 is one of DDR I/O supply inputs (of 2.5V, look at the Datasheet).

It powers the pre-drivers of the DDR IO  pins and can be powered by VDD_HIGH_CAP.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,034件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

  NVCC_DRAM2P5 is one of DDR I/O supply inputs (of 2.5V, look at the Datasheet).

It powers the pre-drivers of the DDR IO  pins and can be powered by VDD_HIGH_CAP.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信