CMA High Latency and allocation failure issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMA High Latency and allocation failure issue

2,401 Views
gauravsuryavans
Contributor II

Hi Community,

I am using imx6 custom board, i am facing CMA latency and allocation failure issue.

Is there any way to reduce latency of CMA allocation ?

Any help would be appreciated.

Regards,

Pankaj

0 Kudos
Reply
2 Replies

2,253 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Pankaj,

There could be several root causes. It could be that you are requiring large memory allocations and this process can increase latency depending on the memory configuration. If this is the case you could try setting a memory region on the device tree for the nodes requiring large amounts of memory, but there is no much information on how to configure this on NXP documentation.

Regards,

0 Kudos
Reply

2,253 Views
gauravsuryavans
Contributor II

Hi gusarambula‌,

I don't want to go with static allocation, CMA has also another issue sometime it will failed to allocate memory, so CMA is not reliable, let me know is there any other options ? 

GCMA and CONFIG_CMA zone are the options available but they have also their own drawback, so thats why they are not in mainline kernel.

Let me know if you know any other way for dynamic allocation ?

Regards,

Pankaj

0 Kudos
Reply