Dear community.
Our customer has question below.
Please tell me the function explanation and default set value of register of CCM described in IMX6DQRM.
CCM_ANALOG_PLL_ARMn
・bit17:LVDS_SEL
・bit18:LVDS_24MHZ_SEL
・bit19:PLL_SEL
CCM_ANALOG_PLL_SYSn
・bit18:PFD_OFFSET_EN
CCM_ANALOG_PLL_AUDIOn
・bit18:PFD_OFFSET_EN
CCM_ANALOG_PLL_VIDEOn
・bit18:PFD_OFFSET_EN
CCM_ANALOG_PLL_ENETn
・bit18:PFD_OFFSET_EN
・bit19:ENABLE_125M
・bit20:ENABLE_100M
Thank you,
Best Regards.
Takashi.
解決済! 解決策の投稿を見る。
Hello Takashi Takahashi,
I received confirmation that in general these are debug or reserved bits that do not need to be programmed by the customer.
CCM_ANALOG_PLL_ARMn
・bit17:LVDS_SEL
・bit18:LVDS_24MHZ_SEL
・bit19:PLL_SEL
In this case the default value is the one shown on the Reference Manual.
CCM_ANALOG_PLL_SYSn
CCM_ANALOG_PLL_AUDIOn
CCM_ANALOG_PLL_VIDEOn
CCM_ANALOG_PLL_ENETn
・bit18:PFD_OFFSET_EN
As for PDF_OFFSET_EN, this is a test bit. PDF stands for Phase Frequency Detector, not Phase Fractional Divider. The purpose of it is to reduce PLL charge pump nonlinearity. It should not be programed and it will be updated on future releases as reserved.
CCM_ANALOG_PLL_ENETn
・bit19:ENABLE_125M
・bit20:ENABLE_100M
The ENABLE_100M and ENABLE_125M bits in CCM_ANALOG_PLL_ENET enable the output of 100MHz clock and 125MHz clock from the ENET PLL, respectively. 100M clock is used for SATA and the 125M clock is used for PCIe.
I hope this information clarifies your concerns!
Regards,
Hello Takashi Takahashi,
I’m looking for more details on these registers. I’ll update this thread as soon as I have more information.
Regards,
Hello Takashi Takahashi,
I received confirmation that in general these are debug or reserved bits that do not need to be programmed by the customer.
CCM_ANALOG_PLL_ARMn
・bit17:LVDS_SEL
・bit18:LVDS_24MHZ_SEL
・bit19:PLL_SEL
In this case the default value is the one shown on the Reference Manual.
CCM_ANALOG_PLL_SYSn
CCM_ANALOG_PLL_AUDIOn
CCM_ANALOG_PLL_VIDEOn
CCM_ANALOG_PLL_ENETn
・bit18:PFD_OFFSET_EN
As for PDF_OFFSET_EN, this is a test bit. PDF stands for Phase Frequency Detector, not Phase Fractional Divider. The purpose of it is to reduce PLL charge pump nonlinearity. It should not be programed and it will be updated on future releases as reserved.
CCM_ANALOG_PLL_ENETn
・bit19:ENABLE_125M
・bit20:ENABLE_100M
The ENABLE_100M and ENABLE_125M bits in CCM_ANALOG_PLL_ENET enable the output of 100MHz clock and 125MHz clock from the ENET PLL, respectively. 100M clock is used for SATA and the 125M clock is used for PCIe.
I hope this information clarifies your concerns!
Regards,