CCM_CLK1_N/P clock configuration problem on I.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CCM_CLK1_N/P clock configuration problem on I.MX6UL

912 次查看
jack_huang1
Contributor III

On the I.MX6UL scheme,in order to make CCM_CLK1_N/P output 66MHz clock, now set the PMU_MISC1N:LVDS1_CLK_SEL source to PFD6 -- REF_PFD6_CLK == PLL2_PFD2_CLK. When set, there is no clock output.

The schematic diagram is as follows(See the attachment):

 

The application is as follows:

// IPG_CLK_ROOT

   

    // 1. CBCMR:PRE_PERIPH_CLK_SEL(01 derive clock from PLL2 PFD2)

    cbcmr_map = (volatile unsigned char *)mmap(NULL, MAP_SIZE, PROT_READ | PROT_WRITE, MAP_SHARED, fd, 0x20C4000);

 

    cbcmr_pre_periph_clk_sel = (volatile unsigned int *)(cbcmr_map + 0x18);

    *cbcmr_pre_periph_clk_sel = (1 << 18); // 396Mhz

   

    // 2. CBCDR:PRE_PERIPH_CLK_SEL(0 PLL2 (pll2_main_clk))

    cbcdr_pre_periph_clk_sel = (volatile unsigned int *)(cbcmr_map + 0x14);

    *cbcdr_pre_periph_clk_sel = (0 << 26); // 396Mhz

   

    // 3. AHB_CLK_ROOT,CBCDR:AHB_PODF (010 Divide by 3)

    *cbcdr_pre_periph_clk_sel = *cbcdr_pre_periph_clk_sel|(2 << 10); // 132Mhz

   

    // 4. IPG_CLK_ROOT :CBCDR:IPG_PODF (01 divide by 2)

    *cbcdr_pre_periph_clk_sel = *cbcdr_pre_periph_clk_sel|(1 << 8); // 66Mhz

 

 

    // 5. set CCM_CLK1_N/P

    // PMU_MISC1N:LVDS1_CLK_SEL (PFD6 — ref_pfd6_clk == pll2_pfd2_clk)

    ccm_clk_p_n = (volatile unsigned int *)(pmu_misc1n_map + 0x160);

    *ccm_clk_p_n = (0x4 << 0); // CCM_CLK1_N/P ouput clk 66Mhz

 

Please check whether this setup is feasible. How does it need to be modified? Thank you

 

0 项奖励
回复
1 回复

895 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jack_huang1

 

was pll2 programmed correctly in the case. In general one can test it in uboot with "mw" command,

it configures correctly pll2 and IPG_CLK_ROOT, AHB_CLK_ROOT..

https://www.denx.de/wiki/publish/DULG/to-delete/UBootCmdGroupMemory.html

 

Best regards
igor

0 项奖励
回复