C_pkg of i.MX25 ibis model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C_pkg of i.MX25 ibis model

Jump to solution
1,348 Views
torus1000
Contributor V

Hi all,

I compared with i.MX25 and i.MX6DQ ibis model.
There was big difference about C_pkg.
I think C_pkg of i.MX25 is too small. (0.21pF << 3.89344pF)

Are both of them correct?  Or which C_pkg is correct?

Thank you.


---
(1)  http://www.freescale.com/webapp/sps/download/license.jsp?colCode=IMX25_IBIS_MODEL

(1)' https://www.freescale.com/webapp/Download?colCode=IMX28IBIS

(2)  https://www.freescale.com/webapp/Download?colCode=IMX6_DQ_IBIS

##########################(1)################################################

|************************************************************************
| IBIS file senna.ibs generated by Viper version: 2008.08.r27
|************************************************************************
|
[IBIS Ver]       3.2
[Comment Char]   |_char
[File Name]      senna.ibs
[File Rev]       REV_Apr8th_2009
[Date]           Wed Apr  8 10:11:04 2009
[Source]         Generated using: Viper
[Notes]          MAPBGA 17x17
[Disclaimer]    
[Copyright]      Copyright (C) 2008 Freescale Semiconductor Ltd.
|
|****************************************************************
|                i.MX25-400MAPBGA17x17               
|****************************************************************
|
[Component]        i.MX25-400MAPBGA17x17
[Manufacturer]     FREESCALE
[Package]
| variable      typ                 min                 max                
R_pkg           356.18m             3.07m               518.52m            
L_pkg           5.20nH              0.09nH              7.90nH             
C_pkg           0.21pF              0.16pF              2.5pF              
|
[Pin] signal_name          model_name           R_pin     L_pin     C_pin   
A10   SD7                  ProgBufferDdr        378.2m    6.01nH    0.19pF  
A12   SD0                  ProgBufferDdr        398.78m   6.02nH    0.23pF  
A13   SD5                  ProgBufferDdr        452.92m   6.1nH     0.22pF  
A14   SDCLK_B              ProgBufferDdr        443.12m   5.96nH    0.23pF  
A15   SDWE                 ProgBufferDdr        435.91m   6.14nH    0.21pF  
...

##########################(2)################################################

|************************************************************************
| IBIS file 21x21_imx6q_consmr_003.ibs generated by Viper version: 2011.06.09
|************************************************************************
|
[IBIS Ver]       4.2
[Comment Char]   |_char
[File Name]      21x21_imx6q_consmr_003.ibs
[File Rev]       003
[Date]           Sun Mar 25 13:48:36 2012
[Source]         FSL Viper 2011.06.09
[Notes]         
[Disclaimer]                             IMPORTANT NOTICE
...
[Copyright]      (C) Copyright Freescale 2004 - 2012, All Rights Reserved.
|
|****************************************************************
|                iMX6Q               
|****************************************************************
|
[Component]        iMX6Q
[Manufacturer]     FREESCALE
[Package]
| variable      typ                 min                 max                
R_pkg           0.3508997           0.0028730           0.895806           
L_pkg           2.62395nH           0.07145nH           5.71558nH          
C_pkg           3.89344pF           0.59645pF           29.3042pF          
|
[Pin] signal_name      model_name   R_pin     L_pin     C_pin   
A2    PCIE_REXT        gpio         0.646088  4.19621nH 1.57274pF
A3    PCIE_TXM         gpio         0.615102  4.09171nH 1.58877pF
A4    GND              GND          NA        NA        NA      
A5    FA_ANA           POWER        0.653689  4.21374nH 1.58401pF
...

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,149 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
4 Replies
1,150 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,149 Views
Yuri
NXP Employee
NXP Employee

  First, maximal value of i.MX25 C_pkg is 2.5 pF (not too little).

Also, we should take into account, that i.MX25 package is not the same as i.MX6 one.

Usually the default package values (R_pkg, L_pkg, C_pkg, specified under [Package])
are used, if corresponding R_pin, L_pin, and C_pin parameters are not declared.

Standard Input Model,includes the following elements:

• Package elements resistance, inductance, and capacitance

• A clamp (Power_Clamp)

• A clamp (GND_Clamp) that is active when the input voltage is below Ground

• Die capacitance of the input


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,149 Views
torus1000
Contributor V

Dear Yuri,

Thank you for reply.

Probably you didn't have time to check each C_pins.
Please comfirm one more time?

Most(243/246) i.MX25 C_pins are less than 0.35pF and only 3 pins(XN,LD1&LDO) exceed 0.4pF such as 0.41,0.75&2.5pF.
Actually average of 243 C_pins calculated as 0.201852pF

(On the other hand, i.MX6Q I/O pins calculated 1.254312568 and VDD pins were 19.94515041pF. Isn't it big difference 0.20 and 1.25?)

Thanks.

0 Kudos
Reply
1,149 Views
Yuri
NXP Employee
NXP Employee

   The capacitance of i.MX25 pins looks as relatively small, but I am afraid, we do not have another
(than published) IBIS models for i.MX25.

Regards,

Yuri.