Hi all,
I compared with i.MX25 and i.MX6DQ ibis model.
There was big difference about C_pkg.
I think C_pkg of i.MX25 is too small. (0.21pF << 3.89344pF)
Are both of them correct? Or which C_pkg is correct?
Thank you.
---
(1) http://www.freescale.com/webapp/sps/download/license.jsp?colCode=IMX25_IBIS_MODEL
(1)' https://www.freescale.com/webapp/Download?colCode=IMX28IBIS
(2) https://www.freescale.com/webapp/Download?colCode=IMX6_DQ_IBIS
##########################(1)################################################
|************************************************************************
| IBIS file senna.ibs generated by Viper version: 2008.08.r27
|************************************************************************
|
[IBIS Ver] 3.2
[Comment Char] |_char
[File Name] senna.ibs
[File Rev] REV_Apr8th_2009
[Date] Wed Apr 8 10:11:04 2009
[Source] Generated using: Viper
[Notes] MAPBGA 17x17
[Disclaimer]
[Copyright] Copyright (C) 2008 Freescale Semiconductor Ltd.
|
|****************************************************************
| i.MX25-400MAPBGA17x17
|****************************************************************
|
[Component] i.MX25-400MAPBGA17x17
[Manufacturer] FREESCALE
[Package]
| variable typ min max
R_pkg 356.18m 3.07m 518.52m
L_pkg 5.20nH 0.09nH 7.90nH
C_pkg 0.21pF 0.16pF 2.5pF
|
[Pin] signal_name model_name R_pin L_pin C_pin
A10 SD7 ProgBufferDdr 378.2m 6.01nH 0.19pF
A12 SD0 ProgBufferDdr 398.78m 6.02nH 0.23pF
A13 SD5 ProgBufferDdr 452.92m 6.1nH 0.22pF
A14 SDCLK_B ProgBufferDdr 443.12m 5.96nH 0.23pF
A15 SDWE ProgBufferDdr 435.91m 6.14nH 0.21pF
...
##########################(2)################################################
|************************************************************************
| IBIS file 21x21_imx6q_consmr_003.ibs generated by Viper version: 2011.06.09
|************************************************************************
|
[IBIS Ver] 4.2
[Comment Char] |_char
[File Name] 21x21_imx6q_consmr_003.ibs
[File Rev] 003
[Date] Sun Mar 25 13:48:36 2012
[Source] FSL Viper 2011.06.09
[Notes]
[Disclaimer] IMPORTANT NOTICE
...
[Copyright] (C) Copyright Freescale 2004 - 2012, All Rights Reserved.
|
|****************************************************************
| iMX6Q
|****************************************************************
|
[Component] iMX6Q
[Manufacturer] FREESCALE
[Package]
| variable typ min max
R_pkg 0.3508997 0.0028730 0.895806
L_pkg 2.62395nH 0.07145nH 5.71558nH
C_pkg 3.89344pF 0.59645pF 29.3042pF
|
[Pin] signal_name model_name R_pin L_pin C_pin
A2 PCIE_REXT gpio 0.646088 4.19621nH 1.57274pF
A3 PCIE_TXM gpio 0.615102 4.09171nH 1.58877pF
A4 GND GND NA NA NA
A5 FA_ANA POWER 0.653689 4.21374nH 1.58401pF
...
Solved! Go to Solution.
First, maximal value of i.MX25 C_pkg is 2.5 pF (not too little).
Also, we should take into account, that i.MX25 package is not the same as i.MX6 one.
Usually the default package values (R_pkg, L_pkg, C_pkg, specified under [Package])
are used, if corresponding R_pin, L_pin, and C_pin parameters are not declared.
Standard Input Model,includes the following elements:
• Package elements resistance, inductance, and capacitance
• A clamp (Power_Clamp)
• A clamp (GND_Clamp) that is active when the input voltage is below Ground
• Die capacitance of the input
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
Thank you for reply.
Probably you didn't have time to check each C_pins.
Please comfirm one more time?
Most(243/246) i.MX25 C_pins are less than 0.35pF and only 3 pins(XN,LD1&LDO) exceed 0.4pF such as 0.41,0.75&2.5pF.
Actually average of 243 C_pins calculated as 0.201852pF
(On the other hand, i.MX6Q I/O pins calculated 1.254312568 and VDD pins were 19.94515041pF. Isn't it big difference 0.20 and 1.25?)
Thanks.
The capacitance of i.MX25 pins looks as relatively small, but I am afraid, we do not have another
(than published) IBIS models for i.MX25.
Regards,
Yuri.