Is there a documented procedure on how to modify the U-boot to allow it to be booted from QSPI flash on the SABRE-SD? All examples, including AN5127, seem to only boot U-boot from the SD-card. I would like to U-boot to be resident and boot from QSPI flash. Please advise as to how this is accomplished.
Hi Andrew,
You could also refer to the following example document:
Customizing MQX applications on i.MX6SX.
Best regards!
/Carlos
Hi Andrew
please look at sect.4.4.1.5 Flashing an ARM® Cortex®-M4 image on QuadSPI
attached document and thread
How to boot imx6 SABRE SD board from qspi NOR flash using MfgTool
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------