Booting U-boot on i.MX6 Solo X from QSPI on SABRE-SD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Booting U-boot on i.MX6 Solo X from QSPI on SABRE-SD

1,852 次查看
andrewwayner
Contributor I

Is there a documented procedure on how to modify the U-boot to allow it to be booted from QSPI flash on the SABRE-SD? All examples, including AN5127, seem to only boot U-boot from the SD-card. I would like to U-boot to be resident and boot from QSPI flash. Please advise as to how this is accomplished.

标签 (1)
0 项奖励
回复
2 回复数

926 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Andrew,

You could also refer to the following example document:

Customizing MQX applications on i.MX6SX.

Best regards!

/Carlos

0 项奖励
回复

926 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Andrew

please look at sect.4.4.1.5 Flashing an ARM® Cortex®-M4 image on QuadSPI

attached document and thread

How to boot imx6 SABRE SD board from qspi NOR flash using MfgTool

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复