Hi igorpadykov,Yuri,MarekVasut
Board : mcimx28evk
Linux : 2.6.35 kernel version
I am getting jffs2 error while booting from spi.
Why it happens?how to solve this?
Regards
Pt
解決済! 解決策の投稿を見る。
Hi Pt
what are error messages ?
Please refer to this FAQ from MTD
http://www.linux-mtd.infradead.org/faq/jffs2.html#L_messages
======================= JFFS2 generates messages, is there a problem?
JFFS2 adopts the philosophy of keeping the user completely appraised of
what is going on.
This can catch out the unwary novice. The following messages can be
moved to a higher log level once you are sure that they are benign.
Empty flash at 0xXXXXXXXX ends at 0xXXXXXXXX This message is generated
if a block of data is partially written. It is generally not a sign of
any problem.
Name CRC failed on node at 0x00b620c8: Read 0x640c8ca3, calculated
0x795111fe or similar message about CRC failures. If you have ever done
unclean reboots - this is harmless.
=======================
Some the messages may be indeed being caused by power cycling the board
without a proper shutdown. Seems this is harmless.
Best regards
igor
Hi Pt
what are error messages ?
Please refer to this FAQ from MTD
http://www.linux-mtd.infradead.org/faq/jffs2.html#L_messages
======================= JFFS2 generates messages, is there a problem?
JFFS2 adopts the philosophy of keeping the user completely appraised of
what is going on.
This can catch out the unwary novice. The following messages can be
moved to a higher log level once you are sure that they are benign.
Empty flash at 0xXXXXXXXX ends at 0xXXXXXXXX This message is generated
if a block of data is partially written. It is generally not a sign of
any problem.
Name CRC failed on node at 0x00b620c8: Read 0x640c8ca3, calculated
0x795111fe or similar message about CRC failures. If you have ever done
unclean reboots - this is harmless.
=======================
Some the messages may be indeed being caused by power cycling the board
without a proper shutdown. Seems this is harmless.
Best regards
igor
Hi
Thanks.
The error messages are:
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0000: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0004: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0008: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf000c: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0010: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0014: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0018: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf001c: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0020: 0x5555 instead
jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00bf0024: 0x5555 instead
Further such events for this erase block will not be printed
VFS: Mounted root (jffs2 filesystem) on device 31:1.
Freeing init memory: 156K
Mounting /proc and /sys
Starting the hotplug events dispatcher udevd
Synthesizing initial hotplug events
JFFS2 notice: (1146) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0cae68.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000004c)
JFFS2 warning: (1146) jffs2_do_read_inode_internal: no data nodes found for ino #79
JFFS2 notice: (1307) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x4b6174.
jffs2_read_inode(): Bogus imode 0 for ino 373
Returned error for crccheck of ino #79. Expect badness...
JFFS2 notice: (1146) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0caee0.
Node totlen on flash (0xffffffff) != totlen from node ref (0x0000004c)
JFFS2 warning: (1146) jffs2_do_read_inode_internal: no data nodes found for ino #80
Returned error for crccheck of ino #80. Expect badness...
JFFS2 notice: (1146) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0caf5c.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000004c)
JFFS2 warning: (1146) jffs2_do_read_inode_internal: no data nodes found for ino #81
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x579bf8.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000004c)
JFFS2 warning: (1151) jffs2_do_read_inode_internal: no data nodes found for ino #569
iget() failed for ino #569
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x75be5c.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000002c)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x75b178.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
Returned error for crccheck of ino #81. Expect badness...
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x75b0f4.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x75b070.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x7578c0.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000002c)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x74c764.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x749d40.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x749d10.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x74682c.
JFFS2 notice: (1146) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0cafd8.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000004c)
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 warning: (1146) jffs2_do_read_inode_internal: no data nodes found for ino #82
Returned error for crccheck of ino #82. Expect badness...
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x74675c.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x743098.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000002c)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x73d0d8.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x73b5c4.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000002c)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x739264.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x735470.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x715730.
Node totlen on flash (0x00000000) != totlen from node ref (0x00000030)
JFFS2 notice: (1146) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x0cb050.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000004c)
JFFS2 notice: (1151) jffs2_get_inode_nodes: Wrong magic bitmask 0x0000 in node header at 0x71299c.
Node totlen on flash (0x00000000) != totlen from node ref (0x0000002c)
JFFS2 warning: (1146) jffs2_do_read_inode_internal: no data nodes found for ino #83
Returned error for crccheck of ino #83. Expect badness...
It continues...
I have attached the log here
Hi Pt
the message "Magic bitmask 0x1985 not found " means that
size of erase block was not set correctly.
you can just ignore them
Best regards
igor
Hi
Ok. Now I am not able to boot from SPI.
It shows rom error code
0x80501003 The file signature or file version is incorrect.
Regards
Pt
I think you did not erase nor-flash, check below
https://lists.yoctoproject.org/pipermail/meta-freescale/2013-August/003989.html
~igor
Hi
I always erase SPI before the sf write.
sf probe 0
sf erase 0x0 0x300000
sf write 0x42000000 0x0 0x300000
Regards
Pt
you can use sf update,
for first installation use erase + write
~igor
Hi
I am using uboot 2009 version .It doesn't have sf update command.
How to solve this "0x80501003 The file signature or file version is incorrect." error?
Booted from SD card and erased flash
---------------------------------------------------------
root@freescale ~$ cat /proc/mtd
dev: size erasesize name
mtd0: 00300000 00010000 "linux-boot-stream"
mtd1: 00d00000 00010000 "rootfs"
root@freescale ~$ mtdinfo /dev/mtd0
mtd0
Name: linux-boot-stream
Type: nor
Eraseblock size: 65536 bytes, 64.0 KiB
Amount of eraseblocks: 48 (3145728 bytes, 3.0 MiB)
Minimum input/output unit size: 1 byte
Sub-page size: 1 byte
Character device major/minor: 90:0
Bad blocks are allowed: false
Device is writable: true
root@freescale ~$ mtdinfo /dev/mtd1
mtd1
Name: rootfs
Type: nor
Eraseblock size: 65536 bytes, 64.0 KiB
Amount of eraseblocks: 208 (13631488 bytes, 13.0 MiB)
Minimum input/output unit size: 1 byte
Sub-page size: 1 byte
Character device major/minor: 90:2
Bad blocks are allowed: false
Device is writable: true
root@freescale ~$ flash_erase /dev/mtd0 0 0
Erasing 64 Kibyte @ 2f0000 -- 100 % complete
root@freescale ~$ flash_erase /dev/mtd1 0 0
Erasing 64 Kibyte @ cf0000 -- 100 % complete
root@freescale ~$ mount -t jffs2 mtd1 /mnt
Cowardly refusing to erase blocks on filesystem with no valid JFFS2 nodes
empty_blocks 0, bad_blocks 0, c->nr_blocks 208
mount: mounting mtd1 on /mnt failed: Input/output error
Then from uboot prompt.I repeated those commands
tftp 0x42000000 imx28_ivt_linux.sb
sf probe 0
sf erase 0x0 0x300000
sf write 0x42000000 0x0 0x300000
Now I am getting H0x80501003...
Regards
Pt
Shortly "0x80501003 The file signature or file version is incorrect." error
means that image is wrong.
~igor
Hi igorpadykov, Yuri, MarekVasut
I have checked the command line. build image again.
Then I boot from sd card and tried to erase the flash using
flash_erase -j /dev/mtd0 0 0
flash_erase -j /dev/mtd1 0 0
The messages shows that the flash is successfully erased.But I don't think so.
When I done this erase command earlier,it took some time to erase flash and mount command works well.
mount -t jffs2 mtd1 /mnt
Now when I tried to mount after erasing, I am getting following error.
root@freescale ~$ mount -t jffs2 mtd1 /mnt
Cowardly refusing to erase blocks on filesystem with no valid JFFS2 nodes
empty_blocks 0, bad_blocks 0, c->nr_blocks 208
mount: mounting mtd1 on /mnt failed: Input/output error.
Then from uboot prompt, I tried sf probe
But first time it failed to initialize SPI
iMX28 U-Boot > sf probe 0
SF: Got idcode ff ff ff ff ff
Failed to initialize SPI flash at 2:0
iMX28 U-Boot > sf probe 0
SF: Got idcode 20 ba 18 10 00
stmicro
SF: Detected N25Q128 with page size 256, total 16777216 bytes
16384 KiB N25Q128 at 2:0 is now current device
Then I erased the SPI and wrote image file to SPI.
Changed the boot mode switch to 0010 and click on reset button.
Getting the previous rom error code: 0x80501003 The file signature or file version is incorrect
What is the reason for this issue?
Yesterday I was faced the same problem.But when I tried these steps today ,It worked well at first time.
Also I am facing an another problem: -
when I "poweroff",it reboots.
Any powering issues?
Regards
Pt
Hi Pt
if it worked first time (factory blank chip), then probably you did not
erase successfully nor after that with flash_erase.
~igor
Hi igorpadykov
The erase command 'sf erase message' shows that it successfully erased the area.
Also I have tried that mtd utils - flash_erase .It also shows that spi flash erased successfully.
But I have noticed something while using flash_erase command.
When I used flash_erase earlier,It had taken some time to erase flash.
But now the erase operation finish very quickly.
What is the reason behind this issue?Why the erase not working properly?
Even though there is some problem in erasing,why the message is showing "erased successfully"?
Regards
Pt A R
Hi Pt A R
I think you should just debug this with oscilloscope
and jtag debugger.
Also one can dump NOR memory and check if it is erased
correctly or not.
>"But now the erase operation finish very quickly."
Probably it checks that memory already has all 0xFF and just skips ?
~igor
Hi igorpadykov
Thanks. I have seen a thread similar to my issue.
I am loading the imx28_ivt_linux.sb to address '0x0'.
My source code doesn't have the structure defined in the reference manual.
Regards
Pt
Hi igorpadykov,
Ok.
I have erased SPI using flash_erase command and then mount jffs2.
Then I used those uboot commands to load linux boot stream image and rootfs on SPI.
Successfully booted up.But now its waiting for
Waiting for root device /dev/mtdblock2...
Actually I have given noinitrd console=ttyAM0,115200 root=/dev/mtdblock1 rootwait rw rootfstype=jffs2 in command line
Regards
Pt
Hi Pt
Probably you did not update kernel boot command
In ltib. Please run ltib and enter new kernel boot command
In ltib.
~igor