Board won't boot from sd card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board won't boot from sd card

Jump to solution
2,325 Views
totalit
Contributor III

I built fsl-image-qt5 and load it on SD card. But the board doesn't proceed initialization after "Normal boot" line and doesn't start autoboot countdown. What's the issue?

Log:

U-Boot 2016.03-mys-6ulx+ga175019 (Dec 02 2021 - 00:45:10 -0800)

CPU: Freescale i.MX6ULL rev1.1 528 MHz (running at 396 MHz)
CPU: Industrial temperature grade (-40C to 115C) at 33C
Reset cause: POR
Board: MYS-MX6ULL 14x14
I2C: ready
DRAM: 256 MiB
force_idle_bus: sda=1 scl=0 sda.gp=0x1d scl.gp=0x1c
NAND: 256 MiB
MMC: FSL_SDHC: 0
Display: TFT43AB (480x272)
Video: 480x272x24
In: serial
Out: serial
Err: serial
Net: FEC0
Normal Boot
=>

 


Here's boot partition contents:

totalit_0-1639063631421.png

 

Labels (3)
0 Kudos
Reply
1 Solution
2,289 Views
totalit
Contributor III

I solved this. The thing is, bootcmd variable in Uboot was not set. I did setenv bootcmd "fatload mmc 0 $loadaddr boot.scr; source $loadaddr"  to place my script at the beginning of boot, so now it works.

View solution in original post

0 Kudos
Reply
3 Replies
2,290 Views
totalit
Contributor III

I solved this. The thing is, bootcmd variable in Uboot was not set. I did setenv bootcmd "fatload mmc 0 $loadaddr boot.scr; source $loadaddr"  to place my script at the beginning of boot, so now it works.

0 Kudos
Reply
2,316 Views
igorpadykov
NXP Employee
NXP Employee

Hi

 

may be recommended to run ddr test

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-6-7-DDR-Stress-Test-Tool/ta-p/11082...

then update image with new ddr calibration coefficients as described in sect.3.2.1 Changing the DCD table for i.MX DDR initialization   i.MX Porting Guide​

 

Best regards
igor

 

 

 

0 Kudos
Reply
2,300 Views
totalit
Contributor III

I run DDR test, wrote new coefficients to u-boot, but it caused no result, I still get "Normal boot".

0 Kudos
Reply