Best way to transfer high speed serial data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Best way to transfer high speed serial data

676 次查看
rlgagliardo
Contributor I

I have a requirement for a 40Mbps data transfer to an i.MX8. I'd like to keep the number of wires/traces to a minimum so serial is preferred. The obvious choices are USB or Ethernet, but I believe those would require CPU interaction as the packets would need to go through a stack before the data could be extracted. Would a MIPI interface be possible? Presumably the data could be DMA'd from this interface and stored until the block could be processed. Thoughts?

Thanks!

0 项奖励
回复
1 回复

598 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Richard

>Would a MIPI interface be possible? 

seems it is also could be used, probably using fpga and imitate some camera.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复