Assistance Required for Configuring A35 Core Frequency on i.MX8QXP MEK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assistance Required for Configuring A35 Core Frequency on i.MX8QXP MEK

256件の閲覧回数
mbamarnath
Contributor I

Hello Team,

I am working with the i.MX8QXP MEK and need to configure the A35 core frequency to 1 GHz from U-Boot for testing purposes. We are planning to run a set of proprietary benchmark applications on our custom RTOS, which is booted from U-Boot, and these tests need to be conducted across various operating frequencies.

Could you please advise on how I can set the A35 core frequency to a specific value from U-Boot? Any guidance or reference to the appropriate documentation for configuring the A35 CPU frequency from U-Boot would be greatly appreciated.

Thank you for your assistance.

Best regards,
Amar

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

222件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

For the linux you can modify in the dts file. For custom RTOS you can ask them to check on the net.

0 件の賞賛
返信

81件の閲覧回数
mbamarnath
Contributor I

Hello Rita,

Sorry for the late reply, our activities were paused for weeks.

Currently the RTOS doesn't configure any CPU frequency by itself instead it relies on the frequency set by the bootloader, in this case uboot.

So, where in u-boot are we configuring the CPU clock?

Regards,

Amar 

0 件の賞賛
返信