Armnn tensorflow-lite vs Tensorflow-lite on Imx8 plus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Armnn tensorflow-lite vs Tensorflow-lite on Imx8 plus

ソリューションへジャンプ
7,408件の閲覧回数
dnozik
Contributor II

Hi ,

1.I working with Imx8 plus board. (zeus-5.4.70-2.3.0)

2.I am testing tensorflow-lite model with Tensorflow-Lite and ArmNN Tensorflow-lite 

3. These inferences use tensoflow-lite from the different versions that cause incompatibility of flatbuffers and compilation error !!!!!!!!!!!

Is there a way to fix it?  it influences all pipe of models train and execution !!!!!!!!!!!!

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
7,365件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Flatbuffers for TFLite is located in: /usr/include/tensorflow/lite/tools/make/downloads/flatbuffers/. You need to include this path when you build TFLite app.

Flatbuffers for ArmNN is located in /usr/include

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
7,402件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello dnozik,

 

The tensorflow in the iMX8 run on the NPU so is running on hardware and is compatible with version 2.1 of tensorflow lite, if you are using another version may result incompatible.

Regards

 

0 件の賞賛
返信
7,384件の閲覧回数
dnozik
Contributor II

Hi, 

any update on that ... it kind of a critical issue for  us !!!

regards,

dima

0 件の賞賛
返信
7,399件の閲覧回数
dnozik
Contributor II

Hi , 

I am compiling my code with your ArmNN and Tesnorflow lite build according to https://source.codeaurora.org/external/imx/meta-imx/tree/meta-ml/recipes-libraries?h=zeus-5.4.70-2.3... 

 

ArmNN using flatbuffers version 1.11

Tensorflow using flatbuffers version 1.12

Both copies on recipe build finish flatbuffers folder into /usr/include .  !!!! So last one to build will set flatbuffers version.

 

So I have a compilation error and now I need to disable one of Inferences in order to run !!!

 

I need the option to use them both !!!

Dima

0 件の賞賛
返信
7,366件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Flatbuffers for TFLite is located in: /usr/include/tensorflow/lite/tools/make/downloads/flatbuffers/. You need to include this path when you build TFLite app.

Flatbuffers for ArmNN is located in /usr/include

Regards

 

0 件の賞賛
返信
7,349件の閲覧回数
dnozik
Contributor II

in my app I only  make this includes for tensorflow lite

// #include "tensorflow/lite/delegates/xnnpack/xnnpack_delegate.h"
// #include "tensorflow/lite/kernels/register.h"
// #include "tensorflow/lite/string_util.h"
// #include "tensorflow/lite/tools/evaluation/utils.h"

there is no flatbuffers include directly !!! tensorflow lite will include flatbuffers in default location usr/include

 

 

0 件の賞賛
返信
7,360件の閲覧回数
dnozik
Contributor II

Yes, thanks.

But why SDK support Tensorflow lite from tensorflow 2.3.1 and armNN with tensorflow from 1.15 . model cannot be executed on both inferences engine.

 

regards.

0 件の賞賛
返信