Apt-get works in yocto?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Apt-get works in yocto?

17,998 Views
georgesapés
Contributor II

I'm developping an embedded Linux over Penbgwyn board. I've installed Linux in my Pengwyn, but apt-get doesn't works. It doesn't found any repository in sources.list.

Anyone can help me?

Labels (1)
Tags (3)
4 Replies

14,597 Views
manjunathjoshi
Contributor V

Hi Amit,

With the mentioned steps in the link, i could get apt-get on core-image-minimal. Even i created a /etc/apt/source.list. It is able to get updated. But when i do apt-get install it is throwing error. Unable to locate package.

Have you ever seen this?

If Install doesn't work, there is very little use of apt-get.

If there is any other way, please let me know.

Regards,

Manju

0 Kudos
Reply

14,597 Views
amittomar
NXP Employee
NXP Employee

Hi George,

Please look in to below thread and link,may help you.

Yocto with a package manager (ex: apt-get)

     https://wiki.yoctoproject.org/wiki/How_do_I

Thanks,

Amit

14,597 Views
alejandrolozan1
NXP Employee
NXP Employee

Thank you Amit, that is very helpful.

Best Regards,

Alejandro

0 Kudos
Reply

14,598 Views
georgesapés
Contributor II

Thanks Amit for your answer, I will try it now and I'll tell you something as soon as possible

Best Regards,

Jordi

0 Kudos
Reply