Hello I successfully used the DDR_Stress_Tester V0.01 with an i.MX53 custom board. I wanted to switch over to V0.042 and to my surprise, it does not work, I always get "open COMx failed" regardless of the com port I try to use. Has anyone been able to use it ?
I decided to try the USB connexion... After fetching an old laptop on Windows XP (to install the antedated USB drivers !), I managed to have the drivers load, I connected the board but nothing shows up in the Device Manager window. I tried a connexion nevertheless. As expected, the communication fails.
Command line :
DDR_Stress_Tester -t mx53 -df CAR1000026631.inc -com 1
Response :
OpenUART:open COM1 failed.
Open com► failed!
other attempt :
Command line :
DDR_Stress_Tester -t mx53 -df CAR1000026631.inc -com 4
Response :
OpenUART:open COM4 failed.
Open com─ failed!
version :
Copyright (c) 2012 Freescale Semiconductor, Inc. All rights reserved.
Version 0.042., built at 11:30:08,Dec 25 2012
OS version : Windows 7 pro SP 1 64 bits
Porcessor : Intel Core i7-4800MQ
Hi Schirrer
I am afraid "Version 0.042" supports only i.MX6, for i.MX53 please
use tool from official product page
Lab and Test Software (2)
DDR Stress tester kit for the i.MX51 and i.MX53 (REV 1)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------