Android A/B Update on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android A/B Update on i.MX6

6,443 Views
samplej
Contributor I

Reading through the available Android documentation it looks like NXP provides support for Android A/B updates on the i.MX8 but not the i.MX6.  Is this due to any limitation on the i.MX6 or should it be possible to add support?

Labels (2)
0 Kudos
Reply
4 Replies

6,246 Views
nbull
Contributor II

Is that the imx6 processor can't do a a/b seamless update or that the software support is there only for the imx8? Is it possible to adjust the software for the imx8 in order for it to work for the imx6 if it isn't a processor limitation?

0 Kudos
Reply

6,420 Views
joanxie
NXP TechSupport
NXP TechSupport

one can refer to the chapter 7 Android Platform Update of enclosed file, which is available for imx6

0 Kudos
Reply

6,420 Views
samplej
Contributor I

Thanks for the reply - I know i.MX6 supports updates, but they are the non A/B style update where you only have 1 image stored.  I need to support the seamless A/B update format where you always have a valid image available to boot from even if an update fails.

0 Kudos
Reply

6,410 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, I checked that imx6 doesn't support a/b system update, only imx8 does

0 Kudos
Reply