Hi,
I'm new to embedded programming and would like to boot the i.MX6 Quad SABRE Smart Devices using following steps.
I'm follow the steps guides given by "@Kris Zawada" on the forum.
Here is my screenshot of my steps and the log data from the debug USB port.
I've manage write the <>.sdcard file to the SD card base on command below and the SD size are 16GB. However on the SABRE board, I've not connect the Mouse and the Keyboard on the USB OTG.
Here is the log file capture on the USB debug port.
U-Boot 2014.04 (Mar 20 2015 - 23:29:57)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 33 C, calibration data: 0x5724cc7d
Reset cause: POR
Board: MX6-SabreSD
I2C: ready
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Found PFUZE100 deviceid=10,revid=21
mmc1 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
mmc1 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
** Unable to read file zImage **
Booting from net ...
FEC Waiting for PHY auto negotiation to complete.. done
BOOTP broadcast 1
DHCP client bound to address 192.168.0.119
Using FEC device
TFTP from server 0.0.0.0; our IP address is 192.168.0.119; sending through gateway 192.168.0.1
Filename 'zImage'.
Load address: 0x12000000
Loading: T T T T T T T T T T
Retry count exceeded; starting again
BOOTP broadcast 1
DHCP client bound to address 192.168.0.119
Using FEC device
TFTP from server 0.0.0.0; our IP address is 192.168.0.119; sending through gateway 192.168.0.1
Filename 'zImage'.
Load address: 0x12000000
Loading: T T T T
Hi,
Attached was the summary of my step which able to run the Yocto using the .sdcard prebuild file.
My next step was to learn how to change the boot up screen picture to my company logo and learn how to build the Linux and run it on SABRE board.
Then would like to write and simple application on Linux for the project application.
Appreciate if you can lead me where I can learn the steps from begining to advance.
Thanks.