Dear All,
We referred to the following part.
http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
- Table 109. Register VSNVSCTL - ADDR 0x6B (P.110)
According to this, the VSNVSVOLT field is 3bit.
However, this default value is 0x80.
We think a description of the default value is mistake.
Would you confirm this?
Best Regards,
Yuuki
解決済! 解決策の投稿を見る。
Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------