About the VSNVSVOLT default value for PF0100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the VSNVSVOLT default value for PF0100

Jump to solution
588 Views
yuuki
Senior Contributor II

Dear All,

We referred to the following part.

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf
- Table 109. Register VSNVSCTL - ADDR 0x6B (P.110)

According to this, the VSNVSVOLT field is 3bit.
However, this default value is 0x80.

We think a description of the default value is mistake.

Would you confirm this?

Best Regards,
Yuuki

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
523 Views
art
NXP Employee
NXP Employee

Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
524 Views
art
NXP Employee
NXP Employee

Yes, you are right, this is the typo in the manual. The actual default value of the VSNVSVOLT field is 0b110 or 0x6.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply