About interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About interrupt

Jump to solution
1,731 Views
goto11
Contributor III

Hello,community

About the following three questions

About IRQ56 to IRQ63 in Table 7-1 of i.MX 7Dual Applications Processor Reference ManualI want to know the register names for enabling / disabling INT7 to INT0?

GPIO1 Combined interrupt indication for GPIO1 signal 0 throughout 15

Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?

Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?

Best Regards,
Goto

Labels (1)
0 Kudos
Reply
1 Solution
1,653 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for enabling / disabling gpio interrupts one can check GPIOx_ICR,

GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)

i.MX 7Dual Applications Processor Reference Manual

>Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?

yes

>Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?

for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)

through GPIO1(15) has enabled interrupt.

"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,654 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

for enabling / disabling gpio interrupts one can check GPIOx_ICR,

GPIOx_IMR registers described in sect.8.3 General Purpose Input/Output (GPIO)

i.MX 7Dual Applications Processor Reference Manual

>Does an interrupt occur if any valid interrupt condition from signal0 to signal15 is met?

yes

>Does the combined interrupt indication also occur under the interrupt condition from INT7 to INT0?

for example "Combined interrupt indication for GPIO1 signal 0 throughout 15" - if any of GPIO1(0)

through GPIO1(15) has enabled interrupt.

"Active HIGH Interrupt from INT7 from GPIO" only if GPIO1(7) interrupt is enabled.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply