Dear All,
Hello.
I have known that VPU frequency can set at 352 MHz in i.MX6DQ.
Is it possible to set 352 MHz in the i.MX6SDL, too?
If it is not possible, how much max frequency is it possible to set in i.MX6SDL?
Best Regards,
Keita
解決済! 解決策の投稿を見る。
HI Keita
with source modifications one can set any
frequency. However I would suggest to work with
default, as freescale BSP releases optimized with this frequency.
Best regards
igor
HI Keita
max. frequency is 333MHz according to Table 18-4. System Clock
Frequency Values i.MX6SDL Reference Manual (rev.2 5/2015),
it is not possible to set it to 352 MHz.
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thank you for your quick response.
>it is not possible to set it to 352 MHz.
Is it possible to set the 333MHz in i.MX6DL with jb4.2.2?
Or, should one use the default VPU freq?
Best Regards,
Keita
HI Keita
with source modifications one can set any
frequency. However I would suggest to work with
default, as freescale BSP releases optimized with this frequency.
Best regards
igor
Dear Igor,
Hello. Thank you very much!
OK. I got it.
Best Regards,
Keita